NXOpen.UF.Draw.ViewInfo Structure¶
NXOpen.UF.Draw.ViewInfo is an alias for NXOpen.UF.DrawViewInfo_Struct
-
class
NXOpen.UF.
DrawViewInfo_Struct
¶ Bases:
object
Refer to UF_DRAW_view_info_s for documentation.
Fields
NXOpen.UF.DrawViewInfo_Struct.ViewStatus |
Active = UF_DRAW_ACTIVE_VIEW, reference = UF_DRAW_REFERENCE_VIEW. |
NXOpen.UF.DrawViewInfo_Struct.AnchorPoint |
The anchor point of the view. |
NXOpen.UF.DrawViewInfo_Struct.ViewScale |
The view scale. |
NXOpen.UF.DrawViewInfo_Struct.UseRefPt |
If true, then used the saved reference point. |
NXOpen.UF.DrawViewInfo_Struct.CleanModelView |
v15.0 No longer used, model views can no longer be cleaned when imported onto a drawing |
NXOpen.UF.DrawViewInfo_Struct.InheritBoundary |
If TRUE, then the drawing view will inherit the model view’s boundary. |
NXOpen.UF.DrawViewInfo_Struct.TransferAnnotation |
If TRUE, annotations are moved from model view to imported drawing view |
NXOpen.UF.DrawViewInfo_Struct.InheritPmi |
If TRUE, then PMI are copied from the model view to the imported drawing view |
NXOpen.UF.DrawViewInfo_Struct.ModelName |
Part name for the view, filespec with path, must not be NULL or empty. |
NXOpen.UF.DrawViewInfo_Struct.ArrangementName |
Name of arrangement, may be ‘0’. |