NXOpen.UF.Draw.TabnotParams Structure¶
NXOpen.UF.Draw.TabnotParams is an alias for NXOpen.UF.DrawTabnotParams_Struct
-
class
NXOpen.UF.
DrawTabnotParams_Struct
¶ Bases:
object
Refer to UF_DRAW_tabnot_params_s for documentation.
Fields
NXOpen.UF.DrawTabnotParams_Struct.Position |
Position of upper left corner of tabular note |
NXOpen.UF.DrawTabnotParams_Struct.RangeStart |
Cell at start of tabular note range. |
NXOpen.UF.DrawTabnotParams_Struct.RangeEnd |
Cell at end of tabular tabular note range. |
NXOpen.UF.DrawTabnotParams_Struct.TitleCell |
Cell used to represent the table’s title, if any. |
NXOpen.UF.DrawTabnotParams_Struct.UgAspectRatio |
UG text aspect ratio |
NXOpen.UF.DrawTabnotParams_Struct.BorderType |
Type of table border to use |
NXOpen.UF.DrawTabnotParams_Struct.BorderWidth |
Width of table border if table_border_type is set to UF_DRAW_tabnot_ b order_type_double |
NXOpen.UF.DrawTabnotParams_Struct.UseTitleCell |
If TRUE, display title_cell as the title |
NXOpen.UF.DrawTabnotParams_Struct.UseGridLines |
If TRUE, display grid lines between cells |
NXOpen.UF.DrawTabnotParams_Struct.UseVertGridLines |
If TRUE, display vertical grid lines between columns |
NXOpen.UF.DrawTabnotParams_Struct.UseHorizGridLines |
If TRUE, display horizontal grid lines between rows |
NXOpen.UF.DrawTabnotParams_Struct.UseRowHdrGridLines |
If TRUE, display a grid line between row header and body of table |
NXOpen.UF.DrawTabnotParams_Struct.UseColHdrGridLines |
If TRUE, display a grid line between column header and body of tbl |
NXOpen.UF.DrawTabnotParams_Struct.AutoSizeCells |
If TRUE, automatically size row heights and column widths to fit tallest/widest text strings in cells |