NXOpen.UF.Draw.BreakoutData Structure¶
NXOpen.UF.Draw.BreakoutData is an alias for NXOpen.UF.DrawBreakoutData_Struct
-
class
NXOpen.UF.
DrawBreakoutData_Struct
¶ Bases:
object
Refer to UF_DRAW_breakout_data_s for documentation.
Fields
NXOpen.UF.DrawBreakoutData_Struct.BasePoint |
Base point on the floor of breakout |
NXOpen.UF.DrawBreakoutData_Struct.ExtrusionVector |
If NULL_TAG, the extrusion vector is perpendicular to the xy plane of the view and points toward the viewer. |
NXOpen.UF.DrawBreakoutData_Struct.NumCurves |
Number of breakout curves |
NXOpen.UF.DrawBreakoutData_Struct.Curves |
Breakout curves |
NXOpen.UF.DrawBreakoutData_Struct.ConstStatus |
Construction status of each breakout curve |
NXOpen.UF.DrawBreakoutData_Struct.CutThruModel |
Cut through the model |
NXOpen.UF.DrawBreakoutData_Struct.HiddenLineHatching |
Hidden line hatching |