NXOpen.UF.Draw.ArrowParms Structure

NXOpen.UF.Draw.ArrowParms is an alias for NXOpen.UF.DrawArrowParms_Struct

class NXOpen.UF.DrawArrowParms_Struct

Bases: object

Refer to UF_DRAW_arrow_parms_s for documentation.

Fields

NXOpen.UF.DrawArrowParms_Struct.Size Arrow size must be greater than 0.
NXOpen.UF.DrawArrowParms_Struct.TotalLength Arrow total length (must be greater than 0) @@ (B in the figure above) @@
NXOpen.UF.DrawArrowParms_Struct.InclAngle Arrow included angle (must be greater than 0) @@( C in the figure above ) @@
NXOpen.UF.DrawArrowParms_Struct.PastPartDist Arrow past part(must be greater than 0) @@ IMG=uf_draw_grf13.gif Figure Arrow Past Part Distance @@
NXOpen.UF.DrawArrowParms_Struct.StubLen Arrow stub length (must be greater than 0) @@ IMG=uf_draw_grf14.gif Figure Stub Length @@
NXOpen.UF.DrawArrowParms_Struct.HeadType Arrow head type UF_DRAW_ansi_arrow = ansi arrow UF_DRAW_iso_arrow = iso arrow @@ IMG=uf_draw_grf15.gif Figure Ansi vs.
NXOpen.UF.DrawArrowParms_Struct.HeadControl Arrow head control (style) (must be greater than 0) UF_DRAW_open_arrowhead UF_DRAW_closed_arrowhead UF_DRAW_filled_arrowhead @@ IMG=uf_draw_grf16.gif Figure Arrowhead Style @@