NXOpen.UF.Disp.SrfanlData Structure¶
NXOpen.UF.Disp.SrfanlData is an alias for NXOpen.UF.DispSrfanlData_Struct
-
class
NXOpen.UF.
DispSrfanlData_Struct
¶ Bases:
object
Refer to UF_DISP_srfanl_data_s for documentation.
Fields
NXOpen.UF.DispSrfanlData_Struct.SpikeLength |
spike length for a hedgehog display |
NXOpen.UF.DispSrfanlData_Struct.RefPlane |
reference plane, point on a plane & normal. Used for ‘sectional radius’ and ‘distance’ display. |
NXOpen.UF.DispSrfanlData_Struct.RefVector |
reference vector, used for ‘normal radius’ and ‘slope’ display |
NXOpen.UF.DispSrfanlData_Struct.MidValue |
mid value of the scalar function data range for GAUSSIAN type |
NXOpen.UF.DispSrfanlData_Struct.ScaleFactor |
scale factor applied to the data range The range of the scalar function in all ‘face analysis’ faces in the NX part is called the ‘data-range’. Some portion of this range is mapped to displayed colors (from red through green to blue). This mapped range is centered at ‘mid_value’ and has size equal to the size of the data_range times the ‘scale_factor’. The ‘mid_value’ and ‘scale_factor’ are directly controllable by the NX user, using sliders on the ‘face analysis’ dialog. This is only for GAUSSIAN type |
NXOpen.UF.DispSrfanlData_Struct.AnalFacetEdgeTol |
This is the facet edge tolerance for shaded display. |
NXOpen.UF.DispSrfanlData_Struct.AnalFacetChordTol |
This is the facet chord distance for shaded display. |
NXOpen.UF.DispSrfanlData_Struct.AnalFacetAngleTol |
This is the facet angle tolerance for shaded display. |
NXOpen.UF.DispSrfanlData_Struct.AnalFacetWidthTol |
Facet width tolerance for analysis display. |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalData |
one of the 11 scalar functions to display UF_DISP_GAUSSIAN_CURVATURE UF_DISP_MEAN_CURVATURE UF_DISP_MINIMUM_CURVATURE UF_DISP_MAXIMUM_CURVATURE UF_DISP_NORMAL_CURVATURE UF_DISP_SECTIONAL_CURVATURE UF_DISP_SLOPE UF_DISP_DISTANCE UF_DISP_U_CURVATURE UF_DISP_V_CURVATURE UF_DISP_REFLECTION |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalFineness |
one of the 6 values of ‘fineness’ UF_DISP_SHADED_COARSE UF_DISP_SHADED_STANDARD UF_DISP_SHADED_FINE UF_DISP_SHADED_EXTRA_FINE UF_DISP_SHADED_ULTRA_FINE UF_DISP_SHADED_CUSTOMIZE_TOL @@ Refer to SAMPLE=uf_disp_tab2.html fineness/shaded tolerance mapping table ENDSAMPLE @@ |
NXOpen.UF.DispSrfanlData_Struct.ReflType |
reflection type values are: UF_DISP_REFL_TYPE_BLACKLINES UF_DISP_REFL_TYPE_BLKWHTLINES UF_DISP_REFL_TYPE_COLOREDLINES UF_DISP_REFL_TYPE_SIMHORIZON UF_DISP_REFL_TYPE_PHOTOHORIZON UF_DISP_REFL_TYPE_USERIMAGE |
NXOpen.UF.DispSrfanlData_Struct.NumReflLines |
The number of reflection lines. |
NXOpen.UF.DispSrfanlData_Struct.ReflHorizVert |
Determines whether to display horizontal, vertical, or all reflection lines values are: UF_DISP_REFL_HORIZ UF_DISP_REFL_VERT UF_DISP_REFL_HORIZ_AND_VERT |
NXOpen.UF.DispSrfanlData_Struct.ThickReflLines |
One of 3 thicknesses of reflection lines UF_DISP_REFL_THIN UF_DISP_REFL_MEDIUM UF_DISP_REFL_THICK |
NXOpen.UF.DispSrfanlData_Struct.Reflectivity |
surface reflectivity (blending) factor. Must be a value between UF_DISP_REFL_REFLECTIVITY_MIN which results in no reflection and UF_DISP_REFL_REFLECTIVITY_MAX, which is the default, where the surface is absolutely reflective. |
NXOpen.UF.DispSrfanlData_Struct.ReflMoveType |
reflection movement type. To use, set it to one of the following types: UF_DISP_REFL_TRANSLATE_HORIZ UF_DISP_REFL_TRANSLATE_VERT UF_DISP_REFL_ROTATE |
NXOpen.UF.DispSrfanlData_Struct.ReflMovePosition |
reflection translation or rotation factor. This is used when the reflection movement type has been set. Must be a value between UF_DISP_REFL_TRANSLATE_MIN and UF_DISP_REFL_TRANSLATE_MAX when refl_move_type is set to translate or between UF_DISP_REFL_ROTATE_ANGLE_MIN and UF_DISP_REFL_ROTATE_ANGLE_MAX when refl_move_type is set to rotate. |
NXOpen.UF.DispSrfanlData_Struct.ReflSmoothLines |
Determines whether reflection lines should be anti-aliased. |
NXOpen.UF.DispSrfanlData_Struct.ReflUserImageFilename |
Stores user specified reflection image file name. |
NXOpen.UF.DispSrfanlData_Struct.NumContours |
Determines the number of displayed contour lines, bet ween 2 and UF_DISP_MAX_CONTOUR_LINES |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalDisplay |
The type of face analysis display for GAUSSIAN: UF_DISP_FRINGE UF_DISP_HEDGEHOG UF_DISP_CONTOUR_LINES |
NXOpen.UF.DispSrfanlData_Struct.LegendColorTypeGaussian |
This is blend/sharp type for GAUSSIAN type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorNumGaussian |
This is number of color option for GAUSSIAN type |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalDisplayMean |
The type of face analysis display for MEAN: UF_DISP_FRINGE UF_DISP_HEDGEHOG UF_DISP_CONTOUR_LINES |
NXOpen.UF.DispSrfanlData_Struct.MidValueMean |
mid value of the scalar function data range for MEAN type |
NXOpen.UF.DispSrfanlData_Struct.ScaleFactorMean |
scale factor applied to the data range for MEAN |
NXOpen.UF.DispSrfanlData_Struct.LegendColorTypeMean |
This is blend/sharp type for MEAN type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorNumMean |
This is number of color option for MEAN type |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalDisplayMax |
The type of face analysis display for MAX: UF_DISP_FRINGE UF_DISP_HEDGEHOG UF_DISP_CONTOUR_LINES |
NXOpen.UF.DispSrfanlData_Struct.MidValueMax |
mid value of the scalar function data range for MAX type |
NXOpen.UF.DispSrfanlData_Struct.ScaleFactorMax |
scale factor applied to the data range for MAX type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorTypeMax |
This is blend/sharp type for MAX type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorNumMax |
This is number of color option for MAX type |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalDisplayMin |
The type of face analysis display for MIN: UF_DISP_FRINGE UF_DISP_HEDGEHOG UF_DISP_CONTOUR_LINES |
NXOpen.UF.DispSrfanlData_Struct.MidValueMin |
mid value of the scalar function data range for MIN type |
NXOpen.UF.DispSrfanlData_Struct.ScaleFactorMin |
scale factor applied to the data range for MIN type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorTypeMin |
This is blend/sharp type for MIN type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorNumMin |
This is number of color option for MIN type |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalDisplayNormal |
The type of face analysis display for NORMAL: UF_DISP_FRINGE UF_DISP_HEDGEHOG UF_DISP_CONTOUR_LINES |
NXOpen.UF.DispSrfanlData_Struct.MidValueNormal |
mid value of the scalar function data range for NORMAL type |
NXOpen.UF.DispSrfanlData_Struct.ScaleFactorNormal |
scale factor applied to the data range for NORMAL type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorTypeNormal |
This is blend/sharp type for NORMAL type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorNumNormal |
This is number of color option for NORMAL type |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalDisplaySec |
The type of face analysis display for SECTIONAL: UF_DISP_FRINGE UF_DISP_HEDGEHOG UF_DISP_CONTOUR_LINES |
NXOpen.UF.DispSrfanlData_Struct.MidValueSec |
mid value of the scalar function data range for SECTIONAL type |
NXOpen.UF.DispSrfanlData_Struct.ScaleFactorSec |
scale factor applied to the data range for SECTIONAL type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorTypeSec |
This is blend/sharp type for SECTIONAL type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorNumSec |
This is number of color option for SECTIONAL type |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalDisplayU |
The type of face analysis display for U: UF_DISP_FRINGE UF_DISP_HEDGEHOG UF_DISP_CONTOUR_LINES |
NXOpen.UF.DispSrfanlData_Struct.MidValueU |
mid value of the scalar function data range for U type |
NXOpen.UF.DispSrfanlData_Struct.ScaleFactorU |
scale factor applied to the data range for U |
NXOpen.UF.DispSrfanlData_Struct.LegendColorTypeU |
This is blend/sharp type for U type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorNumU |
This is number of color option for U type |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalDisplayV |
The type of face analysis display for V: UF_DISP_FRINGE UF_DISP_HEDGEHOG UF_DISP_CONTOUR_LINES |
NXOpen.UF.DispSrfanlData_Struct.MidValueV |
mid value of the scalar function data range for V type |
NXOpen.UF.DispSrfanlData_Struct.ScaleFactorV |
scale factor applied to the data range for V type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorTypeV |
This is blend/sharp type for V type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorNumV |
This is number of color option for V type |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalDisplaySlope |
The type of face analysis display for SLOPE: UF_DISP_FRINGE UF_DISP_HEDGEHOG UF_DISP_CONTOUR_LINES |
NXOpen.UF.DispSrfanlData_Struct.MidValueSlope |
mid value of the scalar function data range for SLOPE type |
NXOpen.UF.DispSrfanlData_Struct.ScaleFactorSlope |
scale factor applied to the data range for SLOPE |
NXOpen.UF.DispSrfanlData_Struct.LegendColorTypeSlope |
This is blend/sharp type for SLOPE type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorNumSlope |
This is number of color option for SLOPE type |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalDisplayDistance |
The type of face analysis display for DISTANCE: UF_DISP_FRINGE UF_DISP_HEDGEHOG UF_DISP_CONTOUR_LINES |
NXOpen.UF.DispSrfanlData_Struct.MidValueDistance |
mid value of the scalar function data range for DISTANCE type |
NXOpen.UF.DispSrfanlData_Struct.ScaleFactorDistance |
scale factor applied to the data range for DISTANCE |
NXOpen.UF.DispSrfanlData_Struct.LegendColorTypeDistance |
This is blend/sharp type for DISTANCE type |
NXOpen.UF.DispSrfanlData_Struct.LegendColorNumDistance |
This is number of color option for DISTANCE type |
NXOpen.UF.DispSrfanlData_Struct.SurfAnalDisplayRefl |
This is the reflection display UF_DISP_REFL_LINES |