NXOpen.UF.Disp.ConeheadAttrbSTag Structure¶
NXOpen.UF.Disp.ConeheadAttrbSTag is an alias for NXOpen.UF.DispConeheadAttrbSTag_Struct
-
class
NXOpen.UF.
DispConeheadAttrbSTag_Struct
¶ Bases:
object
Refer to UF_DISP_conehead_attrb_s_tag for documentation.
Fields
NXOpen.UF.DispConeheadAttrbSTag_Struct.StaffLength |
Length of conehead staff. |
NXOpen.UF.DispConeheadAttrbSTag_Struct.TotalLength |
Length of overall conehead = arrowhead+staff Default is 1.0 |
NXOpen.UF.DispConeheadAttrbSTag_Struct.ConeRadius |
The radius of the arrowhead’s base. |
NXOpen.UF.DispConeheadAttrbSTag_Struct.Color |
The color to draw the vector in, or -1 = Use background Color 0 = Use System Color |
NXOpen.UF.DispConeheadAttrbSTag_Struct.Font |
The display font setting: 1 = Solid 2 = Dashed 3 = Phantom 4 = Centerline 5-7 = User Defined |
NXOpen.UF.DispConeheadAttrbSTag_Struct.Density |
The density settings 0 = Normal 1 = Heavy 2 = Thin |