NXOpen.UF.Cutter.TurnTrackingPointData Structure¶
NXOpen.UF.Cutter.TurnTrackingPointData is an alias for NXOpen.UF.CutterTurnTrackingPointData_Struct
-
class
NXOpen.UF.
CutterTurnTrackingPointData_Struct
¶ Bases:
object
Refer to UF_CUTTER_turn_tracking_point_data_s for documentation.
Fields
NXOpen.UF.CutterTurnTrackingPointData_Struct.Tlangl |
The tool angle of the point |
NXOpen.UF.CutterTurnTrackingPointData_Struct.Radius |
The radius value of the point |
NXOpen.UF.CutterTurnTrackingPointData_Struct.Xoff |
The postprocessor X offset of the point |
NXOpen.UF.CutterTurnTrackingPointData_Struct.Yoff |
The postprocessor Y offset of the point |
NXOpen.UF.CutterTurnTrackingPointData_Struct.Adjust |
The adjust register to use with this point |
NXOpen.UF.CutterTurnTrackingPointData_Struct.Cutcom |
The cutcom register to use with this point |
NXOpen.UF.CutterTurnTrackingPointData_Struct.Radiusid |
The radius id of this point |
NXOpen.UF.CutterTurnTrackingPointData_Struct.Cluster |
The P value of this point |
NXOpen.UF.CutterTurnTrackingPointData_Struct.Name |
The name of the tracking point |