NXOpen.UF.Cutter.TrackingPointData Structure¶
NXOpen.UF.Cutter.TrackingPointData is an alias for NXOpen.UF.CutterTrackingPointData_Struct
-
class
NXOpen.UF.
CutterTrackingPointData_Struct
¶ Bases:
object
Refer to UF_CUTTER_tracking_point_data_s for documentation.
Fields
NXOpen.UF.CutterTrackingPointData_Struct.Diameter |
The output diameter of the point |
NXOpen.UF.CutterTrackingPointData_Struct.Distance |
The distance of the point along the tool axis |
NXOpen.UF.CutterTrackingPointData_Struct.Zoff |
The postprocessor Z offset of the point |
NXOpen.UF.CutterTrackingPointData_Struct.Adjust |
The adjust register to use with this point |
NXOpen.UF.CutterTrackingPointData_Struct.Cutcom |
The cutcom register to use with this point |
NXOpen.UF.CutterTrackingPointData_Struct.ZoffStatus |
The active/inactive status of the Z offset |
NXOpen.UF.CutterTrackingPointData_Struct.AdjustStatus |
The active/inactive status of the adjust register |
NXOpen.UF.CutterTrackingPointData_Struct.CutcomStatus |
The active/inactive status of the cutcom register |
NXOpen.UF.CutterTrackingPointData_Struct.Name |
The name of the tracking point |