NXOpen.UF.Cutlevels.Single StructureΒΆ

NXOpen.UF.Cutlevels.Single is an alias for NXOpen.UF.CutLevelsSingle_Struct

Fields

NXOpen.UF.CutLevelsSingle_Struct.EntityTag Tag id of the face or point entity used to define the current cut level.
NXOpen.UF.CutLevelsSingle_Struct.ZLevel The z distance of the cut level from the origin along the normal of the cut levels.
NXOpen.UF.CutLevelsSingle_Struct.LocalCutDepth The max depth per cut value to be used for the range between this cut level and the one above it.