NXOpen.UF.Curve.WrapData Structure¶
NXOpen.UF.Curve.WrapData is an alias for NXOpen.UF.CurveWrapData_Struct
-
class
NXOpen.UF.
CurveWrapData_Struct
¶ Bases:
object
Refer to UF_CURVE_wrap_data_s for documentation.
Fields
NXOpen.UF.CurveWrapData_Struct.WrapUnwrapSw |
Object type: UF_CURVE_WRAP or UF_CURVE_UNWRAP |
NXOpen.UF.CurveWrapData_Struct.NumWrapFaces |
Number of tags in the wrap_faces array |
NXOpen.UF.CurveWrapData_Struct.WrapFaces |
Conical or cylindrical faces to wrap onto/unwrap from (If multiple faces, they must be on the same cone/cylinder. |
NXOpen.UF.CurveWrapData_Struct.WrapPlane |
Datum plane or face to wrap from/ unwrap onto. |
NXOpen.UF.CurveWrapData_Struct.NumInputCurves |
Number of tags in the input_curves array. |
NXOpen.UF.CurveWrapData_Struct.InputCurves |
Object Identifiers of curves, edges, faces (same as reference to the edges of the face). |
NXOpen.UF.CurveWrapData_Struct.CutLineAngle |
Expression specifying the cut line angle, relative to the tangent line, in degrees 0 - 360. |
NXOpen.UF.CurveWrapData_Struct.DistanceTol |
Distance tolerance to use in calculations e.g. |
NXOpen.UF.CurveWrapData_Struct.AngleTol |
Angle tolerance to use in curve fitting |