NXOpen.UF.Curve.TrimMult Structure¶
NXOpen.UF.Curve.TrimMult is an alias for NXOpen.UF.CurveTrimMult_Struct
-
class
NXOpen.UF.
CurveTrimMult_Struct
¶ Bases:
object
Refer to UF_CURVE_trim_mult_s for documentation.
Fields
NXOpen.UF.CurveTrimMult_Struct.NumBound1Pts |
The number of points in following array. |
NXOpen.UF.CurveTrimMult_Struct.Bound1Pts |
The intersection points of boundary 1, or the single boundary, and the string being trimmed. |
NXOpen.UF.CurveTrimMult_Struct.NumBound2Pts |
The number of points in following array. |
NXOpen.UF.CurveTrimMult_Struct.Bound2Pts |
The intersection points of boundary 2 and the string being trimmed. |