NXOpen.UF.Curve.SectionPerpcrvData Structure¶
NXOpen.UF.Curve.SectionPerpcrvData is an alias for NXOpen.UF.CurveSectionPerpcrvData_Struct
-
class
NXOpen.UF.
CurveSectionPerpcrvData_Struct
¶ Bases:
object
Refer to UF_CURVE_section_perpcrv_data_s for documentation.
Fields
NXOpen.UF.CurveSectionPerpcrvData_Struct.CurveEid |
Curve eid |
NXOpen.UF.CurveSectionPerpcrvData_Struct.Direction |
1 if percentages are from start to end of the curve -1 if opposite direction |
NXOpen.UF.CurveSectionPerpcrvData_Struct.SpaceMeth |
1 for equal parameter spacing, 2 for geometric progression spacing, 3 for chordal tolerance spacing, 4 for incremental arclength spacing |
NXOpen.UF.CurveSectionPerpcrvData_Struct.NumPoints |
Number of points on the curve |
NXOpen.UF.CurveSectionPerpcrvData_Struct.StartPct |
Start percentage on the curve (see direction) |
NXOpen.UF.CurveSectionPerpcrvData_Struct.EndPct |
End percentage on the curve (see direction) |
NXOpen.UF.CurveSectionPerpcrvData_Struct.Ratio |
Ratio for geometric progression spacing |
NXOpen.UF.CurveSectionPerpcrvData_Struct.ChordTol |
Tolerance for chordal toleraance spacing |
NXOpen.UF.CurveSectionPerpcrvData_Struct.Increment |
Increment for incremental arclength spacing |