NXOpen.UF.Curve.SectionGeneralData Structure¶
NXOpen.UF.Curve.SectionGeneralData is an alias for NXOpen.UF.CurveSectionGeneralData_Struct
-
class
NXOpen.UF.
CurveSectionGeneralData_Struct
¶ Bases:
object
Refer to UF_CURVE_section_general_data_s for documentation.
Fields
NXOpen.UF.CurveSectionGeneralData_Struct.Objects |
Array of objects to be sectioned (Bodies, faces, planes, curves) |
NXOpen.UF.CurveSectionGeneralData_Struct.NumObjects |
Number of objects |
NXOpen.UF.CurveSectionGeneralData_Struct.Associate |
1 for associative curves, 0 for non_associative curves (a group of curves is returned) |
NXOpen.UF.CurveSectionGeneralData_Struct.Grouping |
1 if the curves are to be grouped by plane, 0 otherwise (ignored if associate is 1) |
NXOpen.UF.CurveSectionGeneralData_Struct.JoinType |
0 for no joining of the section curves, 1 if the curves are to be joined into cubic polynomial spline curves, 2 if the curves are to be joined into general spline curves, 3 if the curves are to be joined into quintic polynomial spline curves |
NXOpen.UF.CurveSectionGeneralData_Struct.Tolerance |
tolerance (in part units) for the section curves |
NXOpen.UF.CurveSectionGeneralData_Struct.CurveFitData |
curve fit method, max degree & max segments |