NXOpen.UF.Curve.OcfValues Structure

NXOpen.UF.Curve.OcfValues is an alias for NXOpen.UF.CurveOcfValues_Struct

class NXOpen.UF.CurveOcfValues_Struct

Bases: object

Refer to UF_CURVE_ocf_values_s for documentation.

Fields

NXOpen.UF.CurveOcfValues_Struct.String A character string used to hold an offset value in form of a string (e.g “2.0”) to offset the string on the input set of faces.