NXOpen.UF.Curve.LineArc Structure¶
NXOpen.UF.Curve.LineArc is an alias for NXOpen.UF.CurveLineArc_Struct
-
class
NXOpen.UF.
CurveLineArc_Struct
¶ Bases:
object
Refer to UF_CURVE_line_arc_s for documentation.
Fields
NXOpen.UF.CurveLineArc_Struct.CurveType |
Type of curve to create i.e. |
NXOpen.UF.CurveLineArc_Struct.ArcConstraintSubtype |
The subtype of curve |
NXOpen.UF.CurveLineArc_Struct.Constraints |
Array of constraint to be satisfied. |
NXOpen.UF.CurveLineArc_Struct.Limits |
The start and end limits of the curve |
NXOpen.UF.CurveLineArc_Struct.PlaneOfCurve |
Plane on which curve must lie. |
NXOpen.UF.CurveLineArc_Struct.Complement |
False - Default arc will be created. |
NXOpen.UF.CurveLineArc_Struct.Closed |
False - Arc bounded by limits above will be created. |
NXOpen.UF.CurveLineArc_Struct.IsAssociative |
true if associative, false if not associative |