NXOpen.UF.Curve.Limit Structure¶
NXOpen.UF.Curve.Limit is an alias for NXOpen.UF.CurveLimit_Struct
-
class
NXOpen.UF.
CurveLimit_Struct
¶ Bases:
object
Refer to UF_CURVE_limit_s for documentation.
Fields
NXOpen.UF.CurveLimit_Struct.LimitType |
Type of limit |
NXOpen.UF.CurveLimit_Struct.Value |
Value by which to extend * in case of UF_CURVE_limit_value. |
NXOpen.UF.CurveLimit_Struct.LimitingObj |
The object upto which the end must be extended, used when limit type is UF_CURVE_limit_to_entity. |
NXOpen.UF.CurveLimit_Struct.HelpData |
help data when limit type is UF_CURVE_limit_to_entity and there are multiple intersections of line/arc with limiting entity. |