NXOpen.UF.Curve.Constraint Structure¶
NXOpen.UF.Curve.Constraint is an alias for NXOpen.UF.CurveConstraint_Struct
-
class
NXOpen.UF.
CurveConstraint_Struct
¶ Bases:
object
Refer to UF_CURVE_constraint_s for documentation.
Fields
NXOpen.UF.CurveConstraint_Struct.ConstraintType |
The type of constraint |
NXOpen.UF.CurveConstraint_Struct.EndType |
The end to which this constraint * must be applied. |
NXOpen.UF.CurveConstraint_Struct.ObjectTag |
Object with which the constraint * is to be applied. |
NXOpen.UF.CurveConstraint_Struct.Value |
If constraint needs a value then * use this field, ex. |
NXOpen.UF.CurveConstraint_Struct.HelpData |
help data when constraint is tangent / normal |