NXOpen.UF.Curve.BridgeData Structure

NXOpen.UF.Curve.BridgeData is an alias for NXOpen.UF.CurveBridgeData_Struct

class NXOpen.UF.CurveBridgeData_Struct

Bases: object

Refer to UF_CURVE_bridge_data_s for documentation.

Fields

NXOpen.UF.CurveBridgeData_Struct.Method creation method
NXOpen.UF.CurveBridgeData_Struct.InputCurve1 First input string, must contain only one curve or edge.
NXOpen.UF.CurveBridgeData_Struct.InputCurve2 Second input string, must contain only one curve or edge.
NXOpen.UF.CurveBridgeData_Struct.MatchptParms Location parameter on input strings, used as a percentage along the string, must be an expression or a number between 0.0 and 100.0
NXOpen.UF.CurveBridgeData_Struct.MatchPoint Location reference points (optional)
NXOpen.UF.CurveBridgeData_Struct.ReverseTangents True= Reverse Tangents, False = Dont Reverse Tangents
NXOpen.UF.CurveBridgeData_Struct.ShapeControl1 Shape ControlFor UF_CURVE_match_*_ends: Tangent magnitude at first input curve, must be an expression or a number greater than 0.0.
NXOpen.UF.CurveBridgeData_Struct.ShapeControl2 Shape ControlFor UF_CURVE_match_*_ends: Tangent magnatude at second input curve, must be an expression or a number greater than 0.0 For UF_CURVE_match_*_peak: Controls skew at peak point, must be an expression or a number between 0.0 and 100.0
NXOpen.UF.CurveBridgeData_Struct.StiffnessMethod Controls (to some extent) the degree, continuity, and complexity of the curve 0 = automatic 1 = low 2 = high
NXOpen.UF.CurveBridgeData_Struct.InheritCurve Reference shape string, must contain only one curve or edge.