NXOpen.UF.Curve.AnalysisDisplay Structure¶
NXOpen.UF.Curve.AnalysisDisplay is an alias for NXOpen.UF.CurveAnalysisDisplay_Struct
-
class
NXOpen.UF.
CurveAnalysisDisplay_Struct
¶ Bases:
object
Refer to UF_CURVE_analysis_display_s for documentation.
Fields
NXOpen.UF.CurveAnalysisDisplay_Struct.CurvatureCombScaleFactor |
Scale factor to apply to curvature combs - 1.0 is normal. |
NXOpen.UF.CurveAnalysisDisplay_Struct.ShowControlPolygon |
Visible only for splines |
NXOpen.UF.CurveAnalysisDisplay_Struct.ShowCurvatureComb |
Visible for arcs, conics and splines |
NXOpen.UF.CurveAnalysisDisplay_Struct.ShowInflections |
Visible only for splines |
NXOpen.UF.CurveAnalysisDisplay_Struct.ShowPeaks |
Visible only for conics and splines |
NXOpen.UF.CurveAnalysisDisplay_Struct.ShowKnots |
Visible only for splines |
NXOpen.UF.CurveAnalysisDisplay_Struct.CombDensity |
The input teeth of curvature combs |
NXOpen.UF.CurveAnalysisDisplay_Struct.CombInterneedleDensity |
Visibile for arcs, conics and splines |
NXOpen.UF.CurveAnalysisDisplay_Struct.Ustart |
The specified start parameter, range from 0 - 100 |
NXOpen.UF.CurveAnalysisDisplay_Struct.Uend |
The specified end parameter, range from 0 - 100 |
NXOpen.UF.CurveAnalysisDisplay_Struct.UseMaxLength |
Control if limit the max length to combs, true: use max length, otherwise false |
NXOpen.UF.CurveAnalysisDisplay_Struct.MaxLength |
The length to limit combs |
NXOpen.UF.CurveAnalysisDisplay_Struct.ProjChoice |
none=0, plane of curve=1, specified direction=2, work view=3 |
NXOpen.UF.CurveAnalysisDisplay_Struct.SpecifiedDir |
Vector to show which direction the combs will apply to |