NXOpen.UF.Clone.LogFileFailure Structure

NXOpen.UF.Clone.LogFileFailure is an alias for NXOpen.UF.CloneLogFileFailure_Struct

class NXOpen.UF.CloneLogFileFailure_Struct

Bases: object

Refer to UF_CLONE_log_file_failure_s for documentation.

Fields

NXOpen.UF.CloneLogFileFailure_Struct.LineNumber line number in the log file on which the error was detected
NXOpen.UF.CloneLogFileFailure_Struct.InputPartName with UF_free part name being processed when error occurred, may be NULL
NXOpen.UF.CloneLogFileFailure_Struct.InvalidToken with UF_free token which was invalid, may be NULL