NXOpen.UF.Clone.CopyNmOpt Structure

NXOpen.UF.Clone.CopyNmOpt is an alias for NXOpen.UF.CloneCopyNmOpt_Struct

class NXOpen.UF.CloneCopyNmOpt_Struct

Bases: object

Refer to UF_CLONE_copy_nm_opt_s for documentation.

Fields

NXOpen.UF.CloneCopyNmOpt_Struct.NonmasterType when structure is being returned a string containing the name of a nonmaster type defined in the database, such as “specification”
NXOpen.UF.CloneCopyNmOpt_Struct.Copy when structure is being returned a logical indicating whether this nonmaster type should be copied during a clone operation, imported, or exported. TRUE means that nonmasters of that type will be copied