NXOpen.UF.Clear.Summary Structure¶
NXOpen.UF.Clear.Summary is an alias for NXOpen.UF.ClearSummary_Struct
-
class
NXOpen.UF.
ClearSummary_Struct
¶ Bases:
object
Refer to UF_CLEAR_summary_s for documentation.
Fields
NXOpen.UF.ClearSummary_Struct.StartTime |
The starting time of the last analysis run (in seconds since 00:00:00 1/1/1970. |
NXOpen.UF.ClearSummary_Struct.EndTime |
The ending time of the last analysis run (in seconds since 00:00:00 1/1/1970. |
NXOpen.UF.ClearSummary_Struct.RunTime |
the total analysis time (in secs.) |
NXOpen.UF.ClearSummary_Struct.Version |
The version of this analysis run. |
NXOpen.UF.ClearSummary_Struct.AnalysisMode |
The analysis mode. |
NXOpen.UF.ClearSummary_Struct.NumLists |
Number of object lists analyzed. |
NXOpen.UF.ClearSummary_Struct.NList1 |
The number of objects in list 1. |
NXOpen.UF.ClearSummary_Struct.NList2 |
The number of objects in list 2. |
NXOpen.UF.ClearSummary_Struct.NPairs |
The number of pairs built from the object lists. |
NXOpen.UF.ClearSummary_Struct.ExcludedPairs |
The number of pairs that were excluded from analysis, either due to exclusion rules or explicit pair exclusion. |
NXOpen.UF.ClearSummary_Struct.ChangedPairs |
The number of pairs that had changed since the previous clearance analysis. |
NXOpen.UF.ClearSummary_Struct.ChangedObjs |
The number of objects that had changed since the previous clearance analysis. |
NXOpen.UF.ClearSummary_Struct.CheckedPairs |
The total number of pairs that underwent analysis. |
NXOpen.UF.ClearSummary_Struct.NewNHard |
The total number of new hard interferences. |
NXOpen.UF.ClearSummary_Struct.NewNSoft |
The total number of new soft interferences. |
NXOpen.UF.ClearSummary_Struct.NewNTouching |
The total number of new touching interferences. |
NXOpen.UF.ClearSummary_Struct.NewNContainment |
The total number of new containment interferences. |
NXOpen.UF.ClearSummary_Struct.NewNAllInterf |
The total number of new interferences. |
NXOpen.UF.ClearSummary_Struct.NHard |
The total number of hard interferences. |
NXOpen.UF.ClearSummary_Struct.NSoft |
The total number of soft interferences. |
NXOpen.UF.ClearSummary_Struct.NTouching |
The total number of touching interferences. |
NXOpen.UF.ClearSummary_Struct.NContainment |
The total number of containment interferences. |
NXOpen.UF.ClearSummary_Struct.NAllInterf |
The total number of interferences. |
NXOpen.UF.ClearSummary_Struct.JobAborted |
Indicates if the analysis was aborted. |
NXOpen.UF.ClearSummary_Struct.NumZones |
The number of assembly zones used by the analysis (batch only). |