NXOpen.UF.Clear.Pref Structure

NXOpen.UF.Clear.Pref is an alias for NXOpen.UF.ClearPref_Struct

class NXOpen.UF.ClearPref_Struct

Bases: object

Refer to UF_CLEAR_pref_s for documentation.

Fields

NXOpen.UF.ClearPref_Struct.InteractiveMsgFilter The mode of the interactive message filter, composed of one or more of the following bits: UF_CLEAR_NO_INTERFERENCE, UF_CLEAR_SOFT_INTERFERENCE, UF_CLEAR_TOUCH_INTERFERENCE, UF_CLEAR_HARD_INTERFERENCE, UF_CLEAR_CONT_1_IN_2_INTERFERENCE, UF_CLEAR_CONT_2_IN_1_INTERFERENCE, and UF_CLEAR_NEW_INTERFERENCE.
NXOpen.UF.ClearPref_Struct.SaveInterference Should interference bodies be saved?
NXOpen.UF.ClearPref_Struct.InterferenceLayer The layer on which to put interference bodies.
NXOpen.UF.ClearPref_Struct.InterferenceColor The color to assign to all interference bodies.
NXOpen.UF.ClearPref_Struct.InterfAttnColor This member is no longer used.
NXOpen.UF.ClearPref_Struct.ParentAttnColor This member is no longer used.