NXOpen.UF.Clear.InterfData Structure¶
NXOpen.UF.Clear.InterfData is an alias for NXOpen.UF.ClearInterfData_Struct
-
class
NXOpen.UF.
ClearInterfData_Struct
¶ Bases:
object
Refer to UF_CLEAR_interf_data_s for documentation.
Fields
NXOpen.UF.ClearInterfData_Struct.Type |
The type of interference. |
NXOpen.UF.ClearInterfData_Struct.NewInterference |
Is this a new interference? |
NXOpen.UF.ClearInterfData_Struct.NBodies |
The number of interference bodies. |
NXOpen.UF.ClearInterfData_Struct.InterfBodies |
The array of interference body tags. |
NXOpen.UF.ClearInterfData_Struct.Point1 |
A point on object 1. |
NXOpen.UF.ClearInterfData_Struct.Point2 |
A point on object 2. |
NXOpen.UF.ClearInterfData_Struct.Text |
The text associated with this interference. |
NXOpen.UF.ClearInterfData_Struct.InterfNum |
A unique number for the interference. |