NXOpen.UF.Cgm.ExportOptions Structure

NXOpen.UF.Cgm.ExportOptions is an alias for NXOpen.UF.CgmExportOptions_Struct

class NXOpen.UF.CgmExportOptions_Struct

Bases: object

Refer to UF_CGM_export_options_s for documentation.

Fields

NXOpen.UF.CgmExportOptions_Struct.Colors Specifies how colors are applied to exported geometry.
NXOpen.UF.CgmExportOptions_Struct.Widths Specifies how lines widths are applied to exported geometry.
NXOpen.UF.CgmExportOptions_Struct.VdcMode Specifies how coordinates are represented in the CGM file.
NXOpen.UF.CgmExportOptions_Struct.Size Specifies the size or scale of exported geometry.
NXOpen.UF.CgmExportOptions_Struct.TextMode Specifies how text geometry is represented in the CGM file.
NXOpen.UF.CgmExportOptions_Struct.Fonts Specifies how fonts are recorded in the CGM file.
NXOpen.UF.CgmExportOptions_Struct.Reason Specifies the reason the CGM file is being exported.
NXOpen.UF.CgmExportOptions_Struct.Tolerance A unitless value that controls the accuracy or smoothness of exported curve geometry.