NXOpen.UF.Camgeom.CustomPoint Structure¶
NXOpen.UF.Camgeom.CustomPoint is an alias for NXOpen.UF.CamgeomCustomPoint_Struct
-
class
NXOpen.UF.
CamgeomCustomPoint_Struct
¶ Bases:
object
Refer to UF_CAMGEOM_custom_point_s for documentation.
Fields
NXOpen.UF.CamgeomCustomPoint_Struct.PointTag |
tag of defined point - may be null. |
NXOpen.UF.CamgeomCustomPoint_Struct.PointAcs |
point coordinates in Absolute part units. On input, if the point_tag is valid, the coordinates from that entity will be used and this array will be ignored. On output, this array will be filled with the data from the point tag entity if it is specified, otherwise the data from the operation record will be returned. |
NXOpen.UF.CamgeomCustomPoint_Struct.UpperDepth |
The upper depth value. |
NXOpen.UF.CamgeomCustomPoint_Struct.LowerDepth |
The lower depth value. |
NXOpen.UF.CamgeomCustomPoint_Struct.Depth |
The depth value. |