NXOpen.UF.Bound.Tolerance Structure¶
NXOpen.UF.Bound.Tolerance is an alias for NXOpen.UF.BoundTolerance_Struct
-
class
NXOpen.UF.
BoundTolerance_Struct
¶ Bases:
object
Refer to UF_BOUND_tolerance_s for documentation.
Fields
NXOpen.UF.BoundTolerance_Struct.TolSpecified |
Tolerance specified flag: UF_BOUND_NOT_SPECIFIED - not specified UF_BOUND_SPECIFIED - specified |
NXOpen.UF.BoundTolerance_Struct.IntoTolerance |
The maximum allowed tolerance that the boundary may deviate from the defining curves into the part. |
NXOpen.UF.BoundTolerance_Struct.OutTolerance |
The maximum allowed tolerance that the boundary may deviate from the defining curves away from the part. |