NXOpen.UF.Assem.UpgradeStatus Structure

NXOpen.UF.Assem.UpgradeStatus is an alias for NXOpen.UF.AssemUpgradeStatus_Struct

class NXOpen.UF.AssemUpgradeStatus_Struct

Bases: object

Refer to UF_ASSEM_upgrade_status_s for documentation.

Fields

NXOpen.UF.AssemUpgradeStatus_Struct.Failed true if any components could not be upgraded
NXOpen.UF.AssemUpgradeStatus_Struct.NComponents length of the following two arrays
NXOpen.UF.AssemUpgradeStatus_Struct.ComponentNames array of component names that failed to upgrade. This array must be freed using UF_free_string_array.
NXOpen.UF.AssemUpgradeStatus_Struct.Statuses associated statuses with each file name. This array must be freed using UF_free.