NXOpen.UF.Assem.Options Structure¶
NXOpen.UF.Assem.Options is an alias for NXOpen.UF.AssemOptions_Struct
-
class
NXOpen.UF.
AssemOptions_Struct
¶ Bases:
object
Refer to UF_ASSEM_options_s for documentation.
Fields
NXOpen.UF.AssemOptions_Struct.LoadOptions |
Load Options - for native mode only UF_ASSEM_load_from_directory UF_ASSEM_load_from_search_dirs UF_ASSEM_load_as_saved |
NXOpen.UF.AssemOptions_Struct.PartsList |
NOTE: parts_list is no longer used |
NXOpen.UF.AssemOptions_Struct.Update |
Update report setting - UF_ASSEM_no_update_report UF_ASSEM_update_report |
NXOpen.UF.AssemOptions_Struct.Emphasize |
Emphasize setting - UF_ASSEM_do_not_emphasize_wp UF_ASSEM_emphasize_wp |
NXOpen.UF.AssemOptions_Struct.EmphasizeColor |
NOTE: emphasize_color is no longer used |
NXOpen.UF.AssemOptions_Struct.FailureAction |
failure Option value - UF_ASSEM_do_abort_on_failure UF_ASSEM_dont_abort_on_failure |
NXOpen.UF.AssemOptions_Struct.MaintainWorkPart |
NOTE: maintain_work_part is no longer used |
NXOpen.UF.AssemOptions_Struct.LoadLatest |
Load latest version switch UF_ASSEM_load_exact_version UF_ASSEM_load_latest_version |
NXOpen.UF.AssemOptions_Struct.LoadComponents |
Load components option UF_ASSEM_dont_load_components UF_ASSEM_do_load_components UF_ASSEM_use_last_component_set UF_ASSEM_use_last_filter UF_ASSEM_specify_filter |
NXOpen.UF.AssemOptions_Struct.LoadFully |
Full load switchUF_ASSEM_load_components_partially UF_ASSEM_load_components_fully |
NXOpen.UF.AssemOptions_Struct.UseLightweightRepresentations |
Lightweight Representations option UF_ASSEM_do_allow_lightweight_representations UF_ASSEM_dont_allow_lightweight_representations |
NXOpen.UF.AssemOptions_Struct.LoadSubstitution |
Allow Substitution switch UF_ASSEM_dont_allow_substitution UF_ASSEM_do_allow_substitution |
NXOpen.UF.AssemOptions_Struct.ApplyToAllLevels |
Apply reference set defaults to all levels UF_ASSEM_dont_ apply_to_all_levels UF_ASSEM_do_apply_to_all_levels prior to V13, the behavior was UF_ASSEM_dont_apply_to_all_levels. |
NXOpen.UF.AssemOptions_Struct.LoadWaveData |
New option for V14, if load_fully is set to UF_ASSEM_load_components_partially then this allows for components with WAVE data in them to be fully loaded. |
NXOpen.UF.AssemOptions_Struct.LoadWaveParents |
Load Unloaded Wave Parents option. |
NXOpen.UF.AssemOptions_Struct.AutoRegenPfmOption |
Auto regenerate missing part family children option. |
NXOpen.UF.AssemOptions_Struct.ManagedModeLoadOptions |
Load Options - for managed mode only UF_ASSEM_managed_load_by_revision_rule UF_ASSEM_managed_load_as_saved |