NXOpen.UF.Assem.McArrayData Structure

NXOpen.UF.Assem.McArrayData is an alias for NXOpen.UF.AssemMcArrayData_Struct

class NXOpen.UF.AssemMcArrayData_Struct

Bases: object

Refer to UF_ASSEM_mc_array_data_s for documentation.

Fields

NXOpen.UF.AssemMcArrayData_Struct.ArraySubtype A flag indicating which type of array this is.
NXOpen.UF.AssemMcArrayData_Struct.MasterComponent The tag of the master component for this array
NXOpen.UF.AssemMcArrayData_Struct.TemplateComponent The tag of the template component for this array.
NXOpen.UF.AssemMcArrayData_Struct.Dimensions An array of expression tags which determine the size of the array.
NXOpen.UF.AssemMcArrayData_Struct.AxisDefinitions The solid entities (faces, datums, etc) which determine the direction of the array.
NXOpen.UF.AssemMcArrayData_Struct.Offsets An array of expression tags which determine the spacing between array elements.
NXOpen.UF.AssemMcArrayData_Struct.ArrayName The name of the array object.