NXOpen.UF.Assem.IsetArrayData Structure

NXOpen.UF.Assem.IsetArrayData is an alias for NXOpen.UF.AssemIsetArrayData_Struct

class NXOpen.UF.AssemIsetArrayData_Struct

Bases: object

Refer to UF_ASSEM_iset_array_data_s for documentation.

Fields

NXOpen.UF.AssemIsetArrayData_Struct.FeatureIset The tag of the feature iset that the array is based upon.
NXOpen.UF.AssemIsetArrayData_Struct.TemplateComponent The tag of the template component for this array.
NXOpen.UF.AssemIsetArrayData_Struct.Dimensions An array of integers which indicates the size of the array.
NXOpen.UF.AssemIsetArrayData_Struct.ArrayName The name of the array object.