NXOpen.UF.Assem.AssemblyDeformPartData Structure¶
NXOpen.UF.Assem.AssemblyDeformPartData is an alias for NXOpen.UF.AssemAssemblyDeformPartData_Struct
-
class
NXOpen.UF.
AssemAssemblyDeformPartData_Struct
¶ Bases:
object
Refer to UF_ASSEM_deform_part_data_s for documentation.
Fields
NXOpen.UF.AssemAssemblyDeformPartData_Struct.ConvertUnitsOnModifiedParts |
Should units conversion be applied on modified parts |
NXOpen.UF.AssemAssemblyDeformPartData_Struct.ConvertUnitsOnReadOnlyModifiedParts |
Should units conversion be done on read only modified parts |
NXOpen.UF.AssemAssemblyDeformPartData_Struct.PartOccToDeform |
The part occurrence that is being deformed. |
NXOpen.UF.AssemAssemblyDeformPartData_Struct.NumParents |
The number of new references for the external geometry |
NXOpen.UF.AssemAssemblyDeformPartData_Struct.OldParents |
The existing parents that are being replaced with new geometry |
NXOpen.UF.AssemAssemblyDeformPartData_Struct.NewParents |
The new geoemtry for deforming the part |
NXOpen.UF.AssemAssemblyDeformPartData_Struct.NumExpressions |
Number of expressions that are used to deform the part |
NXOpen.UF.AssemAssemblyDeformPartData_Struct.OldExpressions |
The existing expressions that are in the definition of the deformable part |
NXOpen.UF.AssemAssemblyDeformPartData_Struct.NewExpressionValues |
The expression values used to deform the part |
NXOpen.UF.AssemAssemblyDeformPartData_Struct.DeformedFeatureTag |
The deformed feature tag that is created from the deformed part |