AddReusableFeatureBuilder Class |
Represents a NXOpen.Tooling.AddReusableFeatureBuilder |
AddReusableFeatureCollection Class |
Represents a collection of AddReusableFeature |
AddReusablePart Class |
Represents a NXOpen.Tooling.AddReusablePart |
AddReusablePartCollection Class |
Represents a collection of AddReusablePart |
AssemblyDrawingBuilder Class |
Represents a NXOpen.Tooling.AssemblyDrawingBuilder which is used to create or edit the Assembly Drawing. |
AssignPatchBuilder Class |
Represents a builder to be used to add sheet bodies as patch surfaces or delete patch surfaces. |
AssignPatchCollection Class |
Represents a collection of AssignPatch builder |
AutoDieCollection Class |
Represents a collection of Die Design Draw Punch |
AutoDieGroup Class |
Represents a group for Auto Stamping Die |
AutoDimensionBuilder Class |
Represents a NXOpen.Tooling.AutoDimensionBuilder which is used to create or edit the Auto Dimension. |
BackingPadBuilder Class |
Represents a NXOpen.Tooling.BackingPadBuilder which is used to create or delete the Backing Pad. |
BendInsertDesignBuilder Class |
Represents a NXOpen.Tooling.BendInsertDesignBuilder Bend Insert Design is to create inset puch or die for bend . |
BendInsertDesignCollection Class |
Creates a NXOpen.Tooling.BendInsertDesignCollection |
BendOperationBuilder Class |
Represents a NXOpen.Tooling.BendOperationBuilder builder. |
BendOperationCollection Class |
Creates a NXOpen.Tooling.BendOperationBuilder |
BlankGeneratorBuilder Class |
Represents a NXOpen.Tooling.BlankGeneratorBuilder This class is for Blank Generator Design UI |
BlankGeneratorCollection Class |
Creates a NXOpen.Tooling.BlankGeneratorBuilder |
BlankLayoutBuilder Class |
Progressive Die Wizard blank layout builder |
BlankLayoutCollection Class |
Creates a NXOpen.Tooling.BlankLayoutBuilder |
BlankNestingBuilder Class |
Blank Nesting Builder of PDW, EDW and Die Engineering. |
BlankNestingCollection Class |
Creates a NXOpen.Tooling.BlankNestingBuilder |
BlendCurve3DBuilder Class |
Represents a NXOpen.Tooling.BlendCurve3DBuilder builder which implements blend curves in one side where the corner radius is too small. |
BomBuilder Class |
Represents a Tooling::BomBuilder builder |
BomCollection Class |
Represents a collection of Bom |
BomListBuilder Class |
Represents a NXOpen.Tooling.BomListBuilder builder. |
BomListDataProvider Class |
Provides basic data for BOM List. |
BurringInsertBuilder Class |
Progressive Die Wizard builder to design burring punch and die insert |
BurringInsertCollection Class |
Creates a NXOpen.Tooling.BurringInsertCollection |
CAMDataManager Class |
Represents an object that manages cam data objects. |
CaeReuseLibrary Class |
Represents a NXOpen.Tooling.CaeReuseLibrary |
CalculateAreaBuilder Class |
The CalculateArea builder |
CalculateAreaCollection Class |
Represents a collection of CalculateArea builder |
ChangeoverManagementBuilder Class |
Represents a NXOpen.Tooling.ChangeoverManagementBuilder to support changeover workflow management. |
ChannelAdjustBuilder Class |
The builder class for Channel Adjust which assists you to adjust the postion and the length of the channel. |
ChannelAdjustCollection Class |
Creates a ChannelAdjust Collection |
ChannelFittingBuilder Class |
The builder class for Channel Fitting which assists you to add cooling fitting. |
ChannelFittingCollection Class |
Creates a ChannelFitting Collection |
ClearanceManagementBuilder Class |
Progressive Die Wizard builder to management clearances. |
ClearanceManagementCollection Class |
Creates a NXOpen.Tooling.ClearanceManagementCollection |
CloneObject Class |
Represents the clone operation in Add Reusable Component Builder. |
ClonePart Class |
Represents the part inforamtion to be cloned in Add Reusable Component Builder. |
ColorExpressionsBuilder Class |
Represents a NXOpen.Tooling.ColorExpressionsBuilder builder. |
CompDrawingBuilder Class |
Represents a NXOpen.Tooling.CompDrawingBuilder which is used to create or edit the Component Drawing. |
ConceptPositionBuilder Class |
concept position builder for standard part design |
ConceptPositionCollection Class |
Represents a collection of ConceptPosition |
ConcurrentDesignManagementBuilder Class |
Represents a NXOpen.Tooling.ConcurrentDesignManagementBuilder to support concurrent design workflow management. |
CoolingConnectBuilder Class |
The builder class for Cooling connection which assists you to create channel and connect it to other channels. |
CoolingConnectCollection Class |
Creates a CoolingConnect Collection |
CoolingDefineChannelBuilder Class |
The builder class for Cooling Define Channel which assists you to create channels directly. |
CoolingDefineChannelCollection Class |
Creates a CoolingDefineChannel Collection |
CoolingExtendBuilder Class |
The builder class for Channel Extend which assists you to extend the channel. |
CoolingExtendCollection Class |
Creates a CoolingExtend Collection. |
CoolingFittingData Class |
Represents the cooling fitting data in Add Channel Fitting Builder. |
CoolingPatternBuilder Class |
The builder class for Cooling pattern which assists you to create channels with selected curves. |
CoolingPatternCollection Class |
Creates a CoolingPattern Collection |
CopySolidBuilder Class |
Represents a NXOpen.Tooling.CopySolidBuilder builder. |
CornerDesignBuilder Class |
Represents a NXOpen.Tooling.CornerDesignBuilder , Corner Design is to provide tools to make corner. |
CornerDesignCollection Class |
Creates a NXOpen.Tooling.CornerDesignCollection |
CostTableDataProvider Class |
Provides basic data for cost feature table data. |
CreateBoxBuilder Class |
Represents a box creation operation |
CreateBoxCollection Class |
Creates CreateBoxBuilder collection |
DefineCamBuilder Class |
Represents a NXOpen.Tooling.DefineCamBuilder to create different types of cam objects, which are used for kinematic motion |
DefineLifterBuilder Class |
Represents a NXOpen.Tooling.DefineLifterBuilder to create different types of lifter objects, which are used for kinematic motion. |
DefineNeutralFactorBuilder Class |
Represeents a NXOpen.Tooling.DefineNeutralFactorBuilder to define neutral factor according to material and formula in the spreadsheet table. |
DesignTrimToolBuilder Class |
Represents a builder to be used to create Mold Wizard design trim tool. |
DesignTrimToolCollection Class |
Creates a DesignTrimToolCollection class |
DieBaseBuilder Class |
Represents Progressive Die Wizard and Engineering Die Wizard builder to manage die base. |
DieBaseCollection Class |
Creates a NXOpen.Tooling.DieBaseCollection |
DieCavityAndSlugHoleBuilder Class |
Represents die cavity and slug hole builder. |
DieDesDrawDieBuilder Class |
Represents the Die Design draw die management builder, which is to create a draw die by selected sheet body, curve and base plane. |
DieDesDrawPunchBuilder Class |
Die Design draw punch management builder, create a draw die punch by selected sheet body, curve and base plane. |
DieDesPierceInsertBuilder Class |
Represents Die Design Pierce Insert builder. |
DieDesignLowerBinderBuilder Class |
Represents a Lower Binder builder |
DieDesignSettingBuilder Class |
Represents a NXOpen.Tooling.DieDesignSettingBuilder This class is for Die Design Setting UI |
DieDesignSettingCollection Class |
Creates a NXOpen.Tooling.DieDesignSettingBuilder . |
DieDesignTrimPostBuilder Class |
Represents a Trim Post builder |
DieEngDefineProductOrientationBuilder Class |
Die Engineer define product orientation builder. |
DieEngDieTipBuilder Class |
Die Engineer die tip management builder. |
DieEngFormTaskBuilder Class |
Represents a Form Task builder |
DieEngLineupBuilder Class |
Die Engineer lineup management builder. |
DieEngProcessUpdateManagerBuilder Class |
Die Engineer process update manager management builder. |
DieEngStampingCarryoverBuilder Class |
Represents a Stamping Carryover builder |
DieEngStampingOutputBuilder Class |
Represents a Stamping Output builder |
DieEngTrimAngleCheck Class |
Represents a die engineering trim angle check analysis object |
DieEngTrimAngleCheckBuilder Class |
Represents a Trim Angle Check builder |
DieEngTrimTaskBuilder Class |
Die Engineer trim task management builder, create a trim task by selected die tip, trim bounds, start plane and end plane. |
DieInsertBuilder Class |
Represents die insert builder. |
DirectUnbendBuilder Class |
The builder contains all inputs for direct unbend. |
DirectUnfoldBuilder Class |
The builder contains all inputs for direct unfolding. |
DirectUnfoldCollection Class |
Creates a NXOpen.Tooling.DirectUnfoldBuilder |
DrawingSheetNameBuilder Class |
Represents a NXOpen.Tooling.DrawingSheetNameBuilder |
EWDraftingBuilder Class |
Represents the drafting builder which is used to create electrode drafting. |
EWMultiPositionBuilder Class |
Represents the multiple position builder which is used to get transformed electrode heads together. |
EWMultiPositionCollection Class |
Creates EWMultiPosition builder collection |
EdgePatchBuilder Class |
Represents a builder to be used to create edge patch surfaces. |
EdgePatchCollection Class |
Represents a collection of EdgePatch builder |
EjectorPostProcessingBuilder Class |
Represents a builder to be used to create Mold Wizard ejector post processing. |
EjectorPostProcessingCollection Class |
Creates a EjectorPostProcessingCollection class |
EjectorTableBuilder Class |
Represens a ejector table builder. |
EjectorTableData Class |
Represents the ejector table data in Ejector Table Builder. |
ElectrodeBlankBuilder Class |
Design electrode blank builder to create an electrode blank for the selected body. |
ElectrodeCheckingBuilder Class |
Electrode Checking builder to check the touch status of all electrode. |
ElectrodeComponentBuilder Class |
Electrode component builder to install holder and pallet. |
ElectrodeCopyBuilder Class |
The ElectrodeCopy builder |
ElectrodeCopyCollection Class |
Represents a collection of ElectrodeCopy builder |
ElectrodeDeleteBuilder Class |
Electrode delete component builder to remove blank, pallet and holder from assembly. |
ElectrodeDesign Class |
Represents an Electrode Design. |
ElectrodeDesignCollection Class |
Represents a collection of Electrode Design. |
ElectrodeInitializationBuilder Class |
Electrode initialize project builder to creates an electrode design assembly. |
EnlargeSurfaceBuilder Class |
Mold Wizard enlarge surface management builder, trims a enlarged surface to a boundary of edges, curves, datum planes or faces. |
EnlargeSurfaceCollection Class |
Represents a collection of Enlarge Surface |
FaceAttributeBuilder Class |
Represents a builder to be used to create face attribute. |
FaceColorManagementBuilder Class |
Tooling builder to assign and edit color of objects |
FaceColorManagementCollection Class |
Creates a NXOpen.Tooling.FaceColorManagementBuilder |
FaceSplitBuilder Class |
Represents a face split operation |
FaceSplitCollection Class |
Creates Face Split collection |
FamilyMoldBuilder Class |
Creates a Mold Wizard Family Mold builder |
FamilyMoldCollection Class |
Creates a NXOpen.Tooling.FamilyMoldCollection |
FastenerAssemConfigBuilder Class |
Represents a Fastener Assem Config Collection. |
FastenerAssemConfigCollection Class |
Represents a collection of FastenerAssy |
FastenerAssy Class |
Represents a NXOpen.Tooling.FastenerAssy |
FastenerAssyCollection Class |
Represents a collection of FastenerAssy |
FastenerAssyCustomizationBuilder Class |
Fastener assembly customization builder. |
FastenerAssyCustomizationCollection Class |
Represents a collection of FastenerAssyCustomizationBuilder |
FastenerRemoveNodeBuilder Class |
Fastener remove node builder. |
FastenerRemoveNodeCollection Class |
Represents a collection of FastenerRemoveNodeBuilder |
FeatureReferenceSetBuilder Class |
Represents a NXOpen.Tooling.FeatureReferenceSetBuilder builder. |
FlowAnalysisBuilder Class |
Represents the builder which is used to create flow analysis. |
FlowDisplayBuilder Class |
Represents the builder which is used to create flow analysis. |
ForceCalculationBuilder Class |
Represents a NXOpen.Tooling.ForceCalculationBuilder Force Calculation Design is to calculate force of process |
ForceCalculationCollection Class |
Creates a NXOpen.Tooling.ForceCalculationBuilder |
FormingInsertBuilder Class |
Progressive Die Wizard builder to design forming punch and die insert |
FormingInsertCollection Class |
Creates a NXOpen.Tooling.FormingInsertBuilder |
GeneralInsertBuilder Class |
General Insert Design Builder of PDW and EDW. |
GuidedExtensionBuilder Class |
Builder for creating Guided Extension surface in NX |
GuidedExtensionManager Class |
Represents the manager of the GuidedExtension builder |
HemFixerBuilder Class |
Hem Fixer Builder of PDW and EDW. |
HoleDatumSymbolBuilder Class |
Creates hole datum symbol builder for progressive die. |
HoleManufacturingNoteBuilder Class |
Tooling builder for HoleManufacturingNote |
HoleManufacturingNoteCollection Class |
Creates a NXOpen.Tooling.HoleManufacturingNoteBuilder |
HoleReportBuilder Class |
Represents a NXOpen.Tooling.HoleReportBuilder This class is for Hole Report Design UI |
HoleReportCollection Class |
Creates a NXOpen.Tooling.HoleReportBuilder |
InitProjBuilder Class |
Represents a NXOpen.Tooling.InitProjBuilder |
InitProjCollection Class |
Represents a collection of InitProj |
InitProjectBuilder Class |
Mold Wizard initialize project builder |
InitProjectCollection Class |
Represents a collection of InitProject builder |
InsertAuxiliaryBuilder Class |
PDW insert auxiliary builder to design various auxiliaries of insert group |
InsertAuxiliaryCollection Class |
Creates a NXOpen.Tooling.InsertAuxiliaryBuilder |
InsertEditToolsBuilder Class |
Represents a NXOpen.Tooling.InsertEditToolsBuilder which is used to copy or delete the insert edit. |
IntermediateStageBuilder Class |
Represents a NXOpen.Tooling.IntermediateStageBuilder builder. |
IntermediateStageCollection Class |
Creates a NXOpen.Tooling.IntermediateStageBuilder |
LayoutBuilder Class |
Represents a Tooling::LayoutBuilder builder |
LayoutManagementBuilder Class |
Layout Management Builder of Engineering Die Wizard |
LayoutManagementCollection Class |
Creates a NXOpen.Tooling.LayoutManagementBuilder |
LayoutRepositionBuilder Class |
Represents a Tooling::LayoutRepositionBuilder builder |
LsdynaFormAnalysisResultDisplayBuilder Class |
Represents a Ly-Dyna Formability Analysis - Result Display builder |
LsdynaGeometryPreparationBuilder Class |
Stamping Die LS-Dyna integration draw geometry preprare builder. |
LsdynaKfileGeneratorBuilder Class |
Represents LS-Dyna K file builder - K file generator builder |
MWCopySheetsBuilder Class |
Builder for copying sheets in the Mold Wizard application |
MWCopySheetsCollection Class |
Represents a collection of MWCopySheets builder |
MWDefineRegionsBuilder Class |
The MWDefineRegions builder |
MWDefineRegionsCollection Class |
Represents a collection of MWDefineRegions builder |
MWDefineSheetsBuilder Class |
Builder for defining sheets in Mold Wizard |
MWDefineSheetsCollection Class |
Represents a collection of MWDefineSheets builder |
MWDesignGuideLinesBuilder Class |
The builder for designing guide lines in Mold Wizard. |
MWDesignGuideLinesCollection Class |
Represents a collection of MWDesignGuideLines builder |
MWDesignPartingSurfaceBuilder Class |
The builder for designing parting surface in Mold Wizard. |
MWDesignPartingSurfaceCollection Class |
Represents a collection of MWDesignPartingSurface builder |
MWLayoutCollection Class |
Creates Mold Wizard layout collection |
MWMoldedPartValidationBuilder Class |
Represents a builder to be used to perform Molded Part Validation analysis. |
MWMoldedPartValidationManager Class |
Represents a manager of the MWMoldedPartValidation builder |
MWPartingManagerBuilder Class |
Builder for the Parting Manager in the Mold Wizard application |
MWPartingManagerCollection Class |
Represents a collection of MWPartingManager builder |
MWSearchRegionBuilder Class |
The Search Region builder is for defining a region by searching the region faces given a set of seed faces and boundary edges. |
MWSearchRegionCollection Class |
Represents a collection of MWSearchRegion builder |
MWTraversePartingLinesBuilder Class |
Builder for creating parting lines by traversing in the Mold Wizard application |
MWTraversePartingLinesCollection Class |
Represents a collection of the MWTraversePartingLines builder |
ManufacturingGeometryBuilder Class |
Represents a builder to be used to create manufacturing geometry. |
ManufacturingGeometryCollection Class |
Represents a collection of Manufacturing Geometry builder. |
MoldCsysBuilder Class |
Mold Wizard MoldCsys project builder |
MoldCsysCollection Class |
Creates a NXOpen.Tooling.MoldCsysCollection |
MoldDesign Class |
Represents an Mold Design. |
MoldDesignCollection Class |
Represents a collection of Mold Design. |
MoldFeatureRecognitionBuilder Class |
Represents a NXOpen.Tooling.MoldFeatureRecognitionBuilder builder |
MoldFillingBuilder Class |
Builder used to add a gate/runner standard part from fill library, it returns None.
|
MoldInsertBuilder Class |
Mold Wizard mold insert management builder |
MoldInsertCollection Class |
Creates a MoldInsertCollection class |
MoldProcessBuilder Class |
Represents a Tooling::MoldProcessBuilder builder |
MoldProcessCollection Class |
Represents a collection of Mold Process |
MoldwizardManager Class |
Provides create builder methods for Moldwizard. |
MotionSimulationBuilder Class |
Represents a NXOpen.Tooling.MotionSimulationBuilder to support dynamic interference check. |
MotionSimulationCollection Class |
Represents a collection of MotionSimulation. |
ObjectAttributeManagementBuilder Class |
Tooling builder to assign and edit attributes of objects |
ObjectAttributeManagementCollection Class |
Creates a NXOpen.Tooling.ObjectAttributeManagementBuilder |
OffsetCurve3DBuilder Class |
Represents a NXOpen.Tooling.OffsetCurve3DBuilder builder which implements offset curves along a direction with offset distance in three dimension. |
PiercingInsertBuilder Class |
Represents piercing insert builder. |
PiercingInsertCollection Class |
Creates a NXOpen.Tooling.PiercingInsertBuilder |
PiercingInsertMiniToolsBuilder Class |
Represents piercing insert mini tools builder. |
PocketBuilder Class |
Mold Wizard pocket management builder |
PocketCollection Class |
Creates a NXOpen.Tooling.PocketBuilder |
PrebendBuilder Class |
Represents a NXOpen.Tooling.PrebendBuilder builder to divide bend faces. |
ProfileSplitBuilder Class |
The ProfileSplit builder |
ProfileSplitCollection Class |
Represents a collection of ProfileSplit builder |
ProgressiveDieManager Class |
Provides create builder methods for Progressive Die. |
PunchInsertBuilder Class |
Represents punch insert builder. |
QuickDatumCsysBuilder Class |
Represents a NXOpen.Tooling.QuickDatumCsysBuilder builder. |
QuickQuotationBuilder Class |
Progressive Die Wizard builder to create quick quotation. |
QuickQuotationCollection Class |
Creates a NXOpen.Tooling.QuickQuotationBuilder |
ReferenceBlendBuilder Class |
The ReferenceBlend builder |
ReferenceBlendCollection Class |
Creates reference blend collection |
ReliefDesignBuilder Class |
Represents a NXOpen.Tooling.ReliefDesignBuilder Relief Design is to cut relief pocket for forming region . |
ReliefDesignCollection Class |
Creates a NXOpen.Tooling.ReliefDesignBuilder |
RemoveHolesBuilder Class |
Remove Hole is used to patch holes for a solid body. |
RenameAndExportComponentBuilder Class |
Creates rename and export component builder for progressive die. |
ReplaceSolidBuilder Class |
Represents a replace solid operation. |
ReplaceSolidCollection Class |
Creates ReplaceSolidBuilder collection |
ReusableObject Class |
Represents a NXOpen.Tooling.ReusableObject |
ReusableObjectManager Class |
Represents a collection of ReusableObjects |
ReusableObjectPasteBuilder Class |
Represents a NXOpen.Tooling.ReusableObjectPasteBuilder |
ReusablePocketBuilder Class |
Reusable pocket builder. |
ReusablePocketCollection Class |
Represents a collection of ReusablePocketBuilder |
ReusePositioningObjectBuilder Class |
Represents a NXOpen.Tooling.ReusePositioningObjectBuilder |
RunSimulationBuilder Class |
Represents a NXOpen.Tooling.RunSimulationBuilder to animate the model, analyze the collision and reference. |
Runner Class |
Represents a runner feature |
RunnerBuilder Class |
Mold Wizard runner management builder, select curves as runner guide, choose section type and edit section parameters, optional choose boolean type to create runner channel. |
RunnerCollection Class |
Represents a collection of Runner |
SIZERCollection Class |
Represents a collection of SIZER |
SIZERExportBuilder Class |
Exports input parameters for motor selection to SIZER drive design to support the sizing, configuration, and selection of drive components. |
SIZERImportBuilder Class |
Imports results for motor selection from SIZER drive design based on the sizing, configuration, and selection of drive components. |
ScrapDesignBuilder Class |
Represents a scrap design builder |
ScrapDesignCollection Class |
Represents a collection of ScrapDesign |
SectionLineCreationBuilder Class |
Represents a NXOpen.Tooling.SectionLineCreationBuilder which is used to create or edit the section line creation. |
SelectReuseLibraryItemBuilder Class |
Select a part from the reuse library |
SelectReuseLibraryListBuilder Class |
Select a list of objects from the reuse library |
SelectReuseLibraryListItemBuilder Class |
Select reuse library list item |
SelectReuseLibraryListItemBuilderList Class |
Represents a list of objects. |
SetPressModelBuilder Class |
Represents a Tooling.SetPressModelBuilder to set and load the press model. |
SheetMetalFeatureRecognitionBuilder Class |
Represents a NXOpen.Tooling.SheetMetalFeatureRecognitionBuilder builder |
ShimBuilder Class |
Shim Builder of PDW and EDW. |
ShimInnerProfileSetBuilder Class |
This is a seed block of set list. |
ShimInnerProfileSetBuilderList Class |
Represents a list of objects. |
SlugRetentionBuilder Class |
Represents a NXOpen.Tooling.SlugRetentionBuilder which is used to create the Slug Retention. |
SmartScrewUpdateBuilder Class |
Smart Screw Update of MW, PDW and EDW. |
SolidPatchBuilder Class |
Represents a builder to be used to create a solid patch. |
SolidPatchCollection Class |
Represents a collection of SolidPatch builder |
SpecialFormingBuilder Class |
Creates special forming insert builder for progressive die. |
SpecialPiercingInsertBuilder Class |
Creates special piercing insert for progressive die. |
SpecifyBaffleBuilder Class |
Represents a builder to be used to create specify baffle. |
SpecifyBaffleCollection Class |
Represents a collection of Specify Baffle builder |
SpecifyCircuitBuilder Class |
Represents a builder to be used to create specify circuit. |
SpecifyCircuitCollection Class |
Represents a collection of Specify Circuit builder |
SpindleSliderBuilder Class |
Represents a Tooling.SpindleSliderBuilder to create a spindle slider |
SplitInsertBuilder Class |
Creates split insert builder for progressive die. |
SplitSolidBuilder Class |
Represents a builder to be used to split a solid with geometry tools. |
SplitSolidCollection Class |
Creates SplitSolid builder collection |
SpreadsheetData Class |
Represents the spreadsheet data which could be standalone spreadsheet file with special format or be the spreadsheet data from part family template part, the latter format will not have any other data except the name and value in class NXOpen.Tooling.SpreadsheetDataParameter , that means it might not return any result in some methods such as GetDefinedAttributesExpressions. |
SpreadsheetDataParameter Class |
Represents parameter in the spreadsheet. |
StandardPartBuilder Class |
Represents a builder to be used to create Mold Wizard Standard Part. |
StandardPartCollection Class |
Creates a StandardPartCollection class |
StandardPartData Class |
Represents the standard part client data. |
StandardPartPositionBuilder Class |
Represents a StandardPartPositionBuilder to add or edit a standard part in the selected plane with specified position. |
StandardPartPositionCollection Class |
Creates a StandardPartPositionCollection class |
StockSizeBuilder Class |
Represents a Tooling::StockSizeBuilder builder. |
StockSizeCollection Class |
Represents a collection of StockSize |
StripLayoutBuilder Class |
Represents a NXOpen.Tooling.StripLayoutBuilder This class is for Strip Layout Design UI |
StripLayoutCollection Class |
Contains the create functions for builders. |
StripLayoutStationInformationBuilder Class |
Strip Layout Process Description Builder of Tooling. |
StripperVentingBuilder Class |
Stripper Venting Builder of PDW and EDW. |
SubInsertBuilder Class |
The SubInsert builder |
SubInsertCollection Class |
Creates SubInsert builder collection |
ToolingDrawingCollection Class |
Creates a NXOpen.Tooling.CompDrawingBuilder |
ToolingManager Class |
Contains the collection objects for creating and iterating over Reuse Library objects. |
ToolingSession Class |
Represents Tooling session |
TraverseLoopBuilder Class |
The builder class for Traverse Loop component which assists you to select or traverse a string of adjacent curves or edges. |
TraverseLoopCollection Class |
Represents a collection of TraverseLoopbuilder |
TrimMoldComponentsBuilder Class |
Represents a builder to be used to create Mold Wizard trim mold components. |
TrimMoldComponentsCollection Class |
Creates a TrimMoldComponentsCollection class |
TrimRegionBuilder Class |
Mold Wizard trim region management builder, trims a body to a boundary of edges, curves or bodies. |
TrimRegionCollection Class |
Represents a collection of Trim Region |
TrimSolidBuilder Class |
Mold Wizard trim solid management builder, trims bounding box body with region, subtract bounding box with workpiece or keep region and box. |
TrimSolidCollection Class |
Represents a collection of Trim Solid |
UndersizeBuilder Class |
Represents a NXOpen.Tooling.UndersizeBuilder |
UndersizeCollection Class |
Creates a undersize builder |
UnfoldingSimulationBuilder Class |
Unfolding Simulation Builder of PDW and EDW. |
UniversalUnformBuilder Class |
Represents a NXOpen.Tooling.UniversalUnformBuilder builder. |
UnusedFileManagementBuilder Class |
Represents a NXOpen.Tooling.UnusedFileManagementBuilder Unused File Management is to manage the unused files of the project. |
UnusedFileManagementCollection Class |
Creates a NXOpen.Tooling.UnusedFileManagementCollection |
UserDefinedMotionBuilder Class |
Represents a NXOpen.Tooling.UserDefinedMotionBuilder to create user defined motion, which contains linear and rotary motion |
ValidCheckBuilder Class |
This is the JA builder for static interference check |
ValidCheckCollection Class |
Represents a collection of ValidCheck |
WallThicknessCheckerBuilder Class |
Represents a builder to be used to perform wall thickness analysis. |
WallThicknessCheckerManager Class |
Represents the manager of the WallThicknessChecker builder |
WireHoleBuilder Class |
Represents a NXOpen.Tooling.WireHoleBuilder This class is for Wire Hole Design UI |
WireHoleCollection Class |
Creates a NXOpen.Tooling.WireHoleBuilder |
WorkflowManagementCollection Class |
Creates a Workflow Management Collection |
WorkpieceBuilder Class |
Mold Wizard work piece builder |
WorkpieceCollection Class |
Creates a Workpiece Collection |