ValidCheckBuilderSelMode Enumeration¶
NXOpen.Tooling.ValidCheckBuilder.SelMode is an alias for NXOpen.Tooling.ValidCheckBuilderSelMode
-
class
NXOpen.Tooling.
ValidCheckBuilderSelMode
¶ Bases:
object
the selection type, including component and solid body
Enum Members
Enum Member Enum Member Description Component Selection type will be set to component Body Selection type will be set to body -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-