ValidCheckBuilderCheckingType Enumeration¶
NXOpen.Tooling.ValidCheckBuilder.CheckingType is an alias for NXOpen.Tooling.ValidCheckBuilderCheckingType
-
class
NXOpen.Tooling.
ValidCheckBuilderCheckingType
¶ Bases:
object
the checking type, including true body, false body or both
Enum Members
Enum Member Enum Member Description TrueBody True body will be used to do checking FalseBody False body will be used to do checking Both Both types of body will be used to do checking -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-