UserDefinedMotionBuilderRotaryCurveTypes Enumeration¶
NXOpen.Tooling.UserDefinedMotionBuilder.RotaryCurveTypes is an alias for NXOpen.Tooling.UserDefinedMotionBuilderRotaryCurveTypes
-
class
NXOpen.Tooling.
UserDefinedMotionBuilderRotaryCurveTypes
¶ Bases:
object
Specifies the motion curve types when motion type is Rotary
Enum Members
Enum Member Enum Member Description Rotary Rotary motion curve type FromFile Motion curve data read from file type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-