TrimSolidBuilderTypes Enumeration¶
NXOpen.Tooling.TrimSolidBuilder.Types is an alias for NXOpen.Tooling.TrimSolidBuilderTypes
-
class
NXOpen.Tooling.
TrimSolidBuilderTypes
¶ Bases:
object
represents the option to select face or sheet body or manufacturing faces to trim the bounding box.
Enum Members
Enum Member Enum Member Description Face Region with body faces. SheetBody Region with sheet bodies. ManufacturingRegion Region with attribute faces. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-