TrimSolidBuilderTrimSolidAction Enumeration¶
NXOpen.Tooling.TrimSolidBuilder.TrimSolidAction is an alias for NXOpen.Tooling.TrimSolidBuilderTrimSolidAction
-
class
NXOpen.Tooling.
TrimSolidBuilderTrimSolidAction
¶ Bases:
object
represents the action to create trim solid.
Enum Members
Enum Member Enum Member Description Trim Action to do trim. Subtract Action to do subtract. KeepBoxandRegion Action to keep box and region. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-