StripLayoutStationInformationBuilder Class¶
-
class
NXOpen.Tooling.
StripLayoutStationInformationBuilder
¶ Bases:
NXOpen.Builder
Strip Layout Process Description Builder of Tooling.
This builder’s Commit doesn’t produce any objects To create a new instance of this class, use
NXOpen.Tooling.StripLayoutCollection.CreateStripLayoutStationInformationBuilder()
Default values.
Property Value ColorPicker 103 ScaleFactor 1.0 StationNumber One New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ColorPicker | Returns or sets the color picker |
ScaleFactor | Returns or sets the text scale size |
StationInformation | Returns or sets the station information which will be added into specified strip |
StationNumber | Returns or sets the station number to define information |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StripLayoutStationInformationBuilderStationItem Enumeration | Specifies the station items |
Property Detail¶
ColorPicker¶
-
StripLayoutStationInformationBuilder.
ColorPicker
¶ Returns or sets the color picker
-------------------------------------
Getter Method
Signature
ColorPicker
Returns: Return type: Id New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorPicker
Parameters: colorPicker (Id) – New in version NX11.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ScaleFactor¶
-
StripLayoutStationInformationBuilder.
ScaleFactor
¶ Returns or sets the text scale size
-------------------------------------
Getter Method
Signature
ScaleFactor
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScaleFactor
Parameters: scaleFactor (float) – New in version NX11.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
StationInformation¶
-
StripLayoutStationInformationBuilder.
StationInformation
¶ Returns or sets the station information which will be added into specified strip
-------------------------------------
Getter Method
Signature
StationInformation
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StationInformation
Parameters: stationInformation (str) – New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
StationNumber¶
-
StripLayoutStationInformationBuilder.
StationNumber
¶ Returns or sets the station number to define information
-------------------------------------
Getter Method
Signature
StationNumber
Returns: Return type: NXOpen.Tooling.StripLayoutStationInformationBuilderStationItem
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StationNumber
Parameters: stationNumber ( NXOpen.Tooling.StripLayoutStationInformationBuilderStationItem
) –New in version NX11.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
Validate¶
-
StripLayoutStationInformationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.