SpreadsheetDataParameterStatus Enumeration¶
NXOpen.Tooling.SpreadsheetDataParameter.Status is an alias for NXOpen.Tooling.SpreadsheetDataParameterStatus
-
class
NXOpen.Tooling.
SpreadsheetDataParameterStatus
¶ Bases:
object
Represents the different spreadsheet parameter status
Enum Members
Enum Member Enum Member Description Lock User can’t change the value in UI SystemKey This is system key parameter UserKey Key parameter analyzed from spreadsheet search HideStatus Not shown in UI ScaleItem This is a scale item ReadOnly This parameter is read only Modified The parameter value is changed ForceColor If the parameter uses user value, normally it shows in UI in a different color. If this status is set, the parameter value will be shown in the same color. HiddenValue The parameter has value, but it should be hidden to user OptionValue The parameter has multiple value, but not treated as key parameter -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-