SpecifyBaffleBuilderAttributeTypes Enumeration¶
NXOpen.Tooling.SpecifyBaffleBuilder.AttributeTypes is an alias for NXOpen.Tooling.SpecifyBaffleBuilderAttributeTypes
-
class
NXOpen.Tooling.
SpecifyBaffleBuilderAttributeTypes
¶ Bases:
object
Types to specify how to assign attributes to the selected body.
Enum Members
Enum Member Enum Member Description BodyAsChannel Cooling channel attributes assigned to the selected body. BodyAsBaffle Cooling baffle attributes assigned to the selected body. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-