SpecialPiercingInsertBuilderStandardOrUserDefinedTypes Enumeration

NXOpen.Tooling.SpecialPiercingInsertBuilder.StandardOrUserDefinedTypes is an alias for NXOpen.Tooling.SpecialPiercingInsertBuilderStandardOrUserDefinedTypes

class NXOpen.Tooling.SpecialPiercingInsertBuilderStandardOrUserDefinedTypes

Bases: object

Specifies the parent part type.

Enum Members

Enum Member Enum Member Description
Standard
UserDefined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.