SpecialPiercingInsertBuilderNormalDieShoeSlugType Enumeration¶
NXOpen.Tooling.SpecialPiercingInsertBuilder.NormalDieShoeSlugType is an alias for NXOpen.Tooling.SpecialPiercingInsertBuilderNormalDieShoeSlugType
-
class
NXOpen.Tooling.
SpecialPiercingInsertBuilderNormalDieShoeSlugType
¶ Bases:
object
Specifies the type of die shoe slug.
Enum Members
Enum Member Enum Member Description Fillet Die shoe slug type is fillet Rectangle Die shoe slug type is rectangle Circle Die shoe slug type is circle Mickey Die shoe slug type is mickey Clearance Die shoe slug type is clearance SlotVer Die shoe slug type is slot vertical SlotHor Die shoe slug type is slot horizontal NotSet Die shoe slug type is none -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-