SpecialPiercingInsertBuilderNormalBottomBackingPlateSlugType Enumeration¶
NXOpen.Tooling.SpecialPiercingInsertBuilder.NormalBottomBackingPlateSlugType is an alias for NXOpen.Tooling.SpecialPiercingInsertBuilderNormalBottomBackingPlateSlugType
-
class
NXOpen.Tooling.
SpecialPiercingInsertBuilderNormalBottomBackingPlateSlugType
¶ Bases:
object
Specifies the type of bottom plate slug.
Enum Members
Enum Member Enum Member Description Fillet Bottom backing plate slug type is fillet Rectangle Bottom backing plate slug type is rectangle Circle Bottom backing plate slug type is circle Mickey Bottom backing plate slug type is mickey Clearance Bottom backing plate slug type is clearance SlotVer Bottom backing plate slug type is slot vertical SlotHor Bottom backing plate slug type is slot horizontal NotSet Bottom backing plate slug type is none -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-