SolidPatchBuilderSolidPatchType Enumeration¶
NXOpen.Tooling.SolidPatchBuilder.SolidPatchType is an alias for NXOpen.Tooling.SolidPatchBuilderSolidPatchType
-
class
NXOpen.Tooling.
SolidPatchBuilderSolidPatchType
¶ Bases:
object
Settings of the solid patch creation types.
Enum Members
Enum Member Enum Member Description SolidPatch Solid patch type indicates to create solid patch LinkBody Link body type indicates to create link body -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-