ShimBuilderTypes Enumeration

NXOpen.Tooling.ShimBuilder.Types is an alias for NXOpen.Tooling.ShimBuilderTypes

class NXOpen.Tooling.ShimBuilderTypes

Bases: object

Specify the shim operation type.

Enum Members

Enum Member Enum Member Description
AddInsert
EditInsert
DeleteInsert
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.