ShimBuilderParentOption Enumeration

NXOpen.Tooling.ShimBuilder.ParentOption is an alias for NXOpen.Tooling.ShimBuilderParentOption

class NXOpen.Tooling.ShimBuilderParentOption

Bases: object

Specify the parent node.

Enum Members

Enum Member Enum Member Description
NoParent
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.