SetPressModelBuilder Class¶
-
class
NXOpen.Tooling.
SetPressModelBuilder
¶ Bases:
NXOpen.Builder
Represents a
Tooling.SetPressModelBuilder
to set and load the press model.To create a new instance of this class, use
NXOpen.Tooling.AutoDieCollection.CreateSetPressModelBuilder()
Default values.
Property Value StrokesPerMinute 0 New in version NX10.0.2.
Properties¶
Property | Description |
---|---|
NameSuffix | Returns or sets the name suffix add to the press model parts |
PressModelPath | Returns or sets the path to clone available press model |
StrokesPerMinute | Returns or sets the strokes per minute of press model |
Tag | Returns the Tag for this object. |
TargetDirectory | Returns or sets the target directory to store cloned press model |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InitializeAvailablePressModels | Initializes the available press models from press model path |
SetPressModelName | Sets the press model name user selected in the list box |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
NameSuffix¶
-
SetPressModelBuilder.
NameSuffix
¶ Returns or sets the name suffix add to the press model parts
-------------------------------------
Getter Method
Signature
NameSuffix
Returns: Return type: str New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
NameSuffix
Parameters: nameSuffix (str) – New in version NX10.0.2.
License requirements: nx_dievalidation (“DIE VALIDATION”)
PressModelPath¶
-
SetPressModelBuilder.
PressModelPath
¶ Returns or sets the path to clone available press model
-------------------------------------
Getter Method
Signature
PressModelPath
Returns: Return type: str New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
PressModelPath
Parameters: pressModelPath (str) – New in version NX10.0.2.
License requirements: nx_dievalidation (“DIE VALIDATION”)
StrokesPerMinute¶
-
SetPressModelBuilder.
StrokesPerMinute
¶ Returns or sets the strokes per minute of press model
-------------------------------------
Getter Method
Signature
StrokesPerMinute
Returns: Return type: float New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
StrokesPerMinute
Parameters: strokesPerMinute (float) – New in version NX10.0.2.
License requirements: nx_dievalidation (“DIE VALIDATION”)
TargetDirectory¶
-
SetPressModelBuilder.
TargetDirectory
¶ Returns or sets the target directory to store cloned press model
-------------------------------------
Getter Method
Signature
TargetDirectory
Returns: Return type: str New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetDirectory
Parameters: pathName (str) – New in version NX10.0.2.
License requirements: nx_dievalidation (“DIE VALIDATION”)
Method Detail¶
InitializeAvailablePressModels¶
-
SetPressModelBuilder.
InitializeAvailablePressModels
¶ Initializes the available press models from press model path
Signature
InitializeAvailablePressModels(pressModelPath)
Parameters: pressModelPath (str) – New in version NX10.0.2.
License requirements: nx_dievalidation (“DIE VALIDATION”)
SetPressModelName¶
-
SetPressModelBuilder.
SetPressModelName
¶ Sets the press model name user selected in the list box
Signature
SetPressModelName(pressModelName)
Parameters: pressModelName (str) – New in version NX10.0.2.
License requirements: nx_dievalidation (“DIE VALIDATION”)
Validate¶
-
SetPressModelBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.