ScrapDesignBuilderEditScrapType Enumeration¶
NXOpen.Tooling.ScrapDesignBuilder.EditScrapType is an alias for NXOpen.Tooling.ScrapDesignBuilderEditScrapType
-
class
NXOpen.Tooling.
ScrapDesignBuilderEditScrapType
¶ Bases:
object
Specifies the edit type of scraps
Enum Members
Enum Member Enum Member Description Split Splits a scrap by selected curves Merge Merges two scraps into one ApplyMinimumRadius Applies minimum radius to sharp corners of scraps ChangeStation Changes the station number of scraps Delete Deletes scraps Update Updates scraps if there is any design change -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-