RunnerBuilderSectionType Enumeration¶
NXOpen.Tooling.RunnerBuilder.SectionType is an alias for NXOpen.Tooling.RunnerBuilderSectionType
-
class
NXOpen.Tooling.
RunnerBuilderSectionType
¶ Bases:
object
Represents the section type of runner channel.
Enum Members
Enum Member Enum Member Description Circular Use circular section type. Parabolic Use parabolic section type. Trapezoidal Use trapezoidal section type. Hexagonal Use hexagonal section type. SemiCircular Use semicircular section type. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-